FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 > Using RS-232 connection and Ethernet connection together
FAQ
Using RS-232 connection and Ethernet connection together
A GOT2000 series model and a Q06HCPU are connected by RS-232.
I want to connect a Q03UDVCPU to this GOT2000 series model by Ethernet.
How can I set it?
I want to connect a Q03UDVCPU to this GOT2000 series model by Ethernet.
How can I set it?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
The GT27, GT25, or GT21 model (Ethernet connection models) can monitor up to four controllers (four channels) (such as PLC CPU, temperature controller, and inverter) simultaneously by using the multi-channel function.
Since channel 1 of the GOT is used to connect the Q06HCPU, use channel 2 to connect the Q03UDVCPU by Ethernet.
The following describes an example of settings to connect the GOT and the Ethernet port built in the Q03UDVCPU by Ethernet.
* For the GT21 model (Ethernet connection model), up to two controllers (two channels) can be monitored simultaneously.
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH2] from the menu.
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
I/F: Ethernet:Multi
(For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
(For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
GOT Net No.: 1
GOT Station: 18
(2) Select [Common] → [Controller Setting] → [CH2] → [Ethernet Controller Setting] from the menu.
Host: *
Net No.: 1 (example)
Station: 1 (example)
Unit Type: QnUD(P)V/QnUDEH
IP address 192.168.3.39
Port No. 5006
Communication: UDP
(3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
(For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH2] → [Ethernet Setting] from the menu.
GOT IP address: 192.168.3.18
Subnet Mask: 255.255.255.0
2. Configure the following settings in GX Works2.
(1) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] from the menu.
IP address: 192.168.3.39
Subnet Mask Pattern: 255.255.255.0
(2) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] → [Open Setting] from the menu.
Protocol: UDP
Open System: MELSOFT Connection
For the details, refer to the following.
? GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
"5.3 GOT Side Settings"
"5.4 PLC Side Setting"
Since channel 1 of the GOT is used to connect the Q06HCPU, use channel 2 to connect the Q03UDVCPU by Ethernet.
The following describes an example of settings to connect the GOT and the Ethernet port built in the Q03UDVCPU by Ethernet.
* For the GT21 model (Ethernet connection model), up to two controllers (two channels) can be monitored simultaneously.
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH2] from the menu.
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
I/F: Ethernet:Multi
(For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
(For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
GOT Net No.: 1
GOT Station: 18
(2) Select [Common] → [Controller Setting] → [CH2] → [Ethernet Controller Setting] from the menu.
Host: *
Net No.: 1 (example)
Station: 1 (example)
Unit Type: QnUD(P)V/QnUDEH
IP address 192.168.3.39
Port No. 5006
Communication: UDP
(3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
(For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH2] → [Ethernet Setting] from the menu.
GOT IP address: 192.168.3.18
Subnet Mask: 255.255.255.0
2. Configure the following settings in GX Works2.
(1) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] from the menu.
IP address: 192.168.3.39
Subnet Mask Pattern: 255.255.255.0
(2) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] → [Open Setting] from the menu.
Protocol: UDP
Open System: MELSOFT Connection
For the details, refer to the following.
? GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
"5.3 GOT Side Settings"
"5.4 PLC Side Setting"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT2000 Series