FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Gestures available for the document display function
FAQ
Gestures available for the document display function
What gestures are available for the document display function?
Answer
■ PDF file (*1)
・ Swipe: Scrolls the document in the swiped direction (eight directions).
・ Pinch in: Reduces the document size to a desired size (25% to 400%).
・ Pinch out: Enlarges the document size to a desired size (25% to 400%).
(*1) GT Designer3 (GOT2000) Version 1.176H or later is required.
■ Document Converter output file
・ Swipe: Scrolls the document in the swiped direction (eight directions).
・ Pinch in: Reduces the document by one size (large → medium → small) (*2)
・ Pinch out: Enlarges the document by one size (small → medium → large) (*3)
(*2) The document size is reduced to a desired size (25% to 400%) in the following cases.
・ GOT Graphic Ver.1 is used and the graphics accelerator is enabled.
(*3) The document size is enlarged to a desired size (25% to 400%) in the following cases.
・ GOT Graphic Ver.1 is used and the graphics accelerator is enabled.
・ Swipe: Scrolls the document in the swiped direction (eight directions).
・ Pinch in: Reduces the document size to a desired size (25% to 400%).
・ Pinch out: Enlarges the document size to a desired size (25% to 400%).
(*1) GT Designer3 (GOT2000) Version 1.176H or later is required.
■ Document Converter output file
・ Swipe: Scrolls the document in the swiped direction (eight directions).
・ Pinch in: Reduces the document by one size (large → medium → small) (*2)
・ Pinch out: Enlarges the document by one size (small → medium → large) (*3)
(*2) The document size is reduced to a desired size (25% to 400%) in the following cases.
・ GOT Graphic Ver.1 is used and the graphics accelerator is enabled.
(*3) The document size is enlarged to a desired size (25% to 400%) in the following cases.
・ GOT Graphic Ver.1 is used and the graphics accelerator is enabled.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (document display)
- Series
- GOT2000 Series