FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Gesture functions available for the historical trend graph
FAQ
Gesture functions available for the historical trend graph
What gestures are available for the historical trend graph?
Answer
The following gestures are available for the historical trend graph.
◆ GT Designer3 (GOT2000) Version 1.100E or later
・ Tap: Displays the cursor on the tapped position.
・ Swipe along the time axis: Scrolls the historical trend graph by half the page in the swiped direction.
・ Pinch in along the time axis: Reduces the time axis by one size (equivalent to the key code switch FFF9).
・ Pinch out along the time axis: Enlarges the time axis by one size (equivalent to the key code switch FFF8).
* Enlargement and reduction in size in the device value direction (along the vertical axis) with gesture operations are not available.
◆ GT Designer3 (GOT2000) Version 1.100E or later
・ Tap: Displays the cursor on the tapped position.
・ Swipe along the time axis: Scrolls the historical trend graph by half the page in the swiped direction.
・ Pinch in along the time axis: Reduces the time axis by one size (equivalent to the key code switch FFF9).
・ Pinch out along the time axis: Enlarges the time axis by one size (equivalent to the key code switch FFF8).
* Enlargement and reduction in size in the device value direction (along the vertical axis) with gesture operations are not available.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (historical trend graph)
- Series
- GOT2000 Series