Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23458
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 20:48
  • Print

Procedure to use the screen gesture function

How can I start to use the screen gesture function?
Category : 

Answer

Perform the following procedure to use the screen gesture function.

◆ GT Designer3 (GOT2000) Version 1.100E or later
1. Select [Common] - [GOT Type Setting]. Select [Use the gesture function], and click [OK].
2. Place a key code switch (screen gesture mode switching) to switch between the screen gesture mode and normal operation mode in the screen gesture inactive area (a 32-dot area from the top edge of the screen).
3. Touch the key code switch (screen gesture mode switching) placed on the base screen of the GOT.

To display the screen gesture inactive area on the drawing screen, select [Screen] - [Screen Property]. Then, select [Display the screen gesture inactive area], and click [OK].

In addition, to make the drawing process smoother, select [Common] - [GOT Type Setting], and then select [Enable the graphics accelerator].
This setting is available for the following conditions.
 GT Designer3 (GOT2000) Version 1.185T or later and GOT Graphic Ver.1, or GT Designer3 (GOT2000) Version 1.112S or later and 1.181P or earlier

Note that the following restrictions are applied.
  ・ GOT startup may become slower.
  ・ In the screen gesture mode, the object display is not refreshed.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries