FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Disabling the screen gesture function
FAQ
Disabling the screen gesture function
How can I disable the screen gesture function?
Answer
◆ GT Designer3 (GOT2000) Version 1.100E or later
1. Select [Common] - [GOT Type Setting], deselect [Use the gesture function], and click [OK].
* The above setting also disables the object gesture function.
1. Select [Common] - [GOT Type Setting], deselect [Use the gesture function], and click [OK].
* The above setting also disables the object gesture function.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series