FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Enabling/disabling single touch operation for the historical data list display with a device value
FAQ
Enabling/disabling single touch operation for the historical data list display with a device value
Can I enable or disable single touch operation for the historical data list display with a device value?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
Even when single touch operation is enabled in the historical data list display settings, you can enable and disable the operation with the device value (GS1794).
When b1 of Gesture Common Control (GS1794) is on: Single touch operation is disabled.
When b1 of Gesture Common Control (GS1794) is off: Single touch operation is enabled.
Note that when single touch operation is disabled in the historical data list display settings, this signal does not work.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (standard function)
- Series
- GOT2000 Series, GOT3000 Series