Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23463
  • Release Date : 2018/09/14 15:06
  • Update : 2018/10/04 13:12
  • Print

Touch Status External Notification (coordinate) during the screen gesture mode

Are the coordinates of the touch position stored in the touch status external notification device during the screen gesture mode?
Category : 

Answer

The coordinates of the touch position in the touch status external notification device (GS654 and GS655) are not updated during the screen gesture mode (while the frame of the screen gesture active area is shown in bright red).

When you touch an enlarged area after canceling the screen gesture mode, the coordinates equivalent to the normal screen size (100%) are stored.

(Example) After point A moves to point B by a pinch-out operation in the screen gesture mode, when you cancel the screen gesture mode and touch point B, the touch status external notification device stores the coordinates of point A.
 
 
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series

May I have your opinion?

Inquiries