FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Operating the objects with the gesture function using the SoftGOT-GOT link function
FAQ
Operating the objects with the gesture function using the SoftGOT-GOT link function
Can I operate the objects of the GOT with the gesture function using the SoftGOT-GOT link function?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
Answer
You cannot operate the objects of the GOT with the gesture function using the SoftGOT-GOT link function, since GT SoftGOT2000 does not support the gesture function.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), SoftGOT
- Series
- GOT2000 Series, SoftGOT