Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23464
  • Release Date : 2018/09/14 15:06
  • Print

Operating the objects with the gesture function using the SoftGOT-GOT link function

Can I operate the objects of the GOT with the gesture function using the SoftGOT-GOT link function?
Category : 

Answer

You cannot operate the objects of the GOT with the gesture function using the SoftGOT-GOT link function, since GT SoftGOT2000 does not support the gesture function.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), SoftGOT
Series
GOT2000 Series, SoftGOT
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?