Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23467
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:07
  • Print

Screen gesture function while using the GOT remote access function

Can I use the screen gesture function from the VNC client while using the GOT remote access function (VNC server function)?

Category : 

Answer

You cannot use the screen gesture function from the VNC client while using the GOT remote access function (VNC server function). 

If the VNC client obtains the authorization while the GOT is in screen gesture mode or displays the screen enlarged with a pinch-out operation, the GOT cancels screen gesture mode or enlarged screen, and displays the original-sized screen (100%). 
The VNC client also displays the original-sized screen (100%). 
After the authorization is transferred to the GOT, switching to screen gesture mode is enabled on the GOT.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), GOT function (VNC server)
Series
GOT2000 Series, GOT3000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries