FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Screen gesture function while using the GOT remote access function
FAQ
Screen gesture function while using the GOT remote access function
Can I use the screen gesture function from the VNC client while using the GOT remote access function (VNC server function)?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
You cannot use the screen gesture function from the VNC client while using the GOT remote access function (VNC server function).
If the VNC client obtains the authorization while the GOT is in screen gesture mode or displays the screen enlarged with a pinch-out operation, the GOT cancels screen gesture mode or enlarged screen, and displays the original-sized screen (100%).
The VNC client also displays the original-sized screen (100%).
After the authorization is transferred to the GOT, switching to screen gesture mode is enabled on the GOT.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (VNC server)
- Series
- GOT2000 Series, GOT3000 Series