Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23486
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:38
  • Print

Gesture function

Answer

The gesture function includes the screen gesture function and object gesture function.

The screen gesture function allows you to zoom in and out on the base screen with pinch-in and pinch-out gestures, and to scroll the base screen with a swipe or slide. 
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.

The object gesture function allows you to zoom in and out on the time axis of a graph or document with pinch-in or pinch-out gestures, and to scroll through graph and document pages with a swipe or slide. 
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with pinch-in and pinch-out gestures.
 

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series, GOT3000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries