Start main contents
Font Size
S
M
L
FAQ
>
Visualization
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
Using with the GOT1000 series on the ...
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
/category/show/2167
Human-Machine Interfaces(HMIs)-GOT
(437)
GOT2000 Series
(400)
GOT1000 Series
(23)
GT SoftGOT
(6)
Engineering Software
(8)
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
No : 23488
Release Date : 2018/09/14 15:06
Update : 2018/09/25 18:00
Print
Using with the GOT1000 series on the network
Can the GOT1000 series and GOT2000 series be used together on the network?
Category :
FAQ
>
Visualization
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
FAQ
>
Visualization
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT27
FAQ
>
Visualization
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT25
FAQ
>
Visualization
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT21
Answer
The GOT1000 series and GOT2000 series can be used together on the network if the network type is one of the following.
・ MELSECNET/H
・ CC-Link IE Controller Network
・ CC-Link IE Field Network
・ CC-Link (Intelligent device station/via G4)
・ Ethernet
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series
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
Operating by touching the screen with...
System language of the GOT2000 series
Use of commercially available SD memo...
Replacing the backlight of the GOT200...
Use of the Ethernet cable
page top
HOME
FAQ