FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 > Using with the GOT1000 series on the network
FAQ
Using with the GOT1000 series on the network
Can the GOT1000 series and GOT2000 series be used together on the network?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
The GOT1000 series and GOT2000 series can be used together on the network if the network type is one of the following.
・ MELSECNET/H
・ CC-Link IE Controller Network
・ CC-Link IE Field Network
・ CC-Link (Intelligent device station/via G4)
・ Ethernet
・ MELSECNET/H
・ CC-Link IE Controller Network
・ CC-Link IE Field Network
・ CC-Link (Intelligent device station/via G4)
・ Ethernet
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT2000 Series