FAQ


FAQAbout Products
 
 - FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Use of a commercially available USB cable for the GOT2000 series
FAQ
Use of a commercially available USB cable for the GOT2000 series
What commercially available USB cables can be used for the GOT2000 series?
    - Category :
- 
      - FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
 
Answer
While you can use commercially available USB cables for the GOT2000 series, we have guaranteed the operation only when one of the following cables is used.
・ GT09-C30USB-5P
・ GT09-C20USB-5P (discontinued)
・ MR-J3USBCBL3M
 
  ・ GT09-C30USB-5P
・ GT09-C20USB-5P (discontinued)
・ MR-J3USBCBL3M
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Cable
- Series
- GOT2000 Series