FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Assigning a USB memory drive for the GOT2000 series
FAQ
Assigning a USB memory drive for the GOT2000 series
When I install a USB memory in a GOT2000 series model, which drive is assigned?
Answer
The GOT2000 series can assign USB drives as follows.

For the details of the drive configuration, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"1.2.7 Drive configuration of the target GOT for data transfer"

For the details of the drive configuration, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"1.2.7 Drive configuration of the target GOT for data transfer"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (standard function)
- Series
- GOT2000 Series