FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Assigning a USB memory drive for the GOT2000 series
FAQ
Assigning a USB memory drive for the GOT2000 series
When I install a USB memory in a GOT2000 series model, which drive is assigned?
Answer
The GOT2000 series can assign USB drives as follows.
For the details of the drive configuration, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"1.2.7 Drive configuration of the target GOT for data transfer"
For the details of the drive configuration, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"1.2.7 Drive configuration of the target GOT for data transfer"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (standard function)
- Series
- GOT2000 Series
May I have your opinion?
Related FAQ
- Changing the bus connection to the Ethernet connection
- Use of commercially available USB memories for the GOT2000 series
- Using with the GOT1000 series in a bus topology
- Trial use of the remote personal computer operation function (Ethernet)
- Transferring data between a personal computer and a GOT via a PLC