FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Use of commercially available USB memories for the GOT2000 series
FAQ
Use of commercially available USB memories for the GOT2000 series
Can I use commercially available USB memories for the GOT2000 series?
Answer
You can use commercially available USB memories for the GOT2000 series.
Note that we do not guarantee the operation when commercially available USB memories are used.
For the details, refer to the following Technical News.
List of Valid Devices Applicable for GOT2000 Series (GOT-A-0064)
Note that we do not guarantee the operation when commercially available USB memories are used.
For the details, refer to the following Technical News.
List of Valid Devices Applicable for GOT2000 Series (GOT-A-0064)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Peripheral (data storage)
- Series
- GOT2000 Series