FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Connecting the GOT2000 series and a barcode reader or other devices by USB
FAQ
Connecting the GOT2000 series and a barcode reader or other devices by USB
Can I connect a GOT2000 series model with a barcode reader, 2D code reader, or RFID by USB?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
You can connect a GOT2000 series model with a barcode reader or 2D code reader by USB.
RFID does not support USB connection.
Note that a barcode reader or 2D code reader to be connected to a GOT2000 series model is required to satisfy the following conditions.
・ A USB keyboard interface is provided.
・ A Japanese 106 keyboard or the English 101 keyboard is settable as the USB keyboard type.
・ "Enter" is settable as the terminator.
Also, GT Designer3 (GOT2000) Version 1.175H or later is required.
Version 1.170C and earlier do not support USB connection with a barcode reader, 2D code reader, or RFID.
RFID does not support USB connection.
Note that a barcode reader or 2D code reader to be connected to a GOT2000 series model is required to satisfy the following conditions.
・ A USB keyboard interface is provided.
・ A Japanese 106 keyboard or the English 101 keyboard is settable as the USB keyboard type.
・ "Enter" is settable as the terminator.
Also, GT Designer3 (GOT2000) Version 1.175H or later is required.
Version 1.170C and earlier do not support USB connection with a barcode reader, 2D code reader, or RFID.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Peripheral, GOT function (communication)
- Series
- GOT2000 Series