FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Transferring data between a personal computer and a GOT via a PLC
FAQ
Transferring data between a personal computer and a GOT via a PLC
Can the GOT screen data be read and written from and to a personal computer via a PLC?
Answer
The GOT screen data can be read and written from and to a personal computer via a PLC.
Note that the following items have restrictions.
・ Connection type between the personal computer and PLC
・ Connection type between the GOT and PLC
・ Type of the PLC to be routed
・ GT Designer3 (GOT2000) version
The following items have restrictions depending on the type of the PLC to be routed.
・ Serial number of the PLC
・ Version of the engineering software (GX Works2)
For the details, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"4.4 Transferring the Data between the Personal Computer and the GOT via PLC CPU"
Note that the following items have restrictions.
・ Connection type between the personal computer and PLC
・ Connection type between the GOT and PLC
・ Type of the PLC to be routed
・ GT Designer3 (GOT2000) version
The following items have restrictions depending on the type of the PLC to be routed.
・ Serial number of the PLC
・ Version of the engineering software (GX Works2)
For the details, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"4.4 Transferring the Data between the Personal Computer and the GOT via PLC CPU"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (screen data transfer)
- Series
- GOT2000 Series