FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Device data transfer between devices connected to the GOT
FAQ
Device data transfer between devices connected to the GOT
When Mitsubishi Electric and non-Mitsubishi Electric PLCs are connected to a GOT2000 series model, how can the device data of each PLC be transferred easily?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
Answer
The GOT2000 series allows device data to be transferred among multiple controllers (among PLCs, PLCs and temperature controllers, etc.).
For the details of the device data transfer function, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"9.4 Transferring Data between Devices ([Device Data Transfer])"
For the details of the device data transfer function, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"9.4 Transferring Data between Devices ([Device Data Transfer])"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (multi-channel function), GOT function (device data transfer)
- Series
- GOT2000 Series