FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Simultaneous 2-point press on the touch panel of the GOT2000 series
FAQ
Simultaneous 2-point press on the touch panel of the GOT2000 series
Is the simultaneous 2-point press available on the touch panel of the GOT2000 series?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
Answer
The simultaneous 2-point press is available on the touch panel of GT27.
However, placement of switches for the simultaneous 2-point press has restrictions.
The simultaneous 2-point press is not supported by GT25 and GT21.
For the details of restrictions, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"8.2.3 Precautions for a touch switch"
However, placement of switches for the simultaneous 2-point press has restrictions.
The simultaneous 2-point press is not supported by GT25 and GT21.
For the details of restrictions, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"8.2.3 Precautions for a touch switch"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT, GOT function (standard function)
- Series
- GOT2000 Series