Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23505
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 17:28
  • Print

Simultaneous 2-point press on the touch panel of the GOT2000 series

Answer

The simultaneous 2-point press is available on the touch panel of GT27.
However, placement of switches for the simultaneous 2-point press has restrictions.
The simultaneous 2-point press is not supported by GT25 and GT21.

For the details of restrictions, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"8.2.3 Precautions for a touch switch"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT, GOT function (standard function)
Series
GOT2000 Series

May I have your opinion?

Inquiries