FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Support of GT Converter2 by the GOT2000 series
FAQ
Support of GT Converter2 by the GOT2000 series
Does GT Converter2 Version 3 support the GOT2000 series?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > Engineering Software > Converter
Answer
◆ GT Converter2 Version 3.12N or earlier
It does not support the GOT2000 series. To use the project data for GOT800 or other series with the GOT2000 series, perform the following operations.
1. Convert the project data into GOT1000 series project data using GT Converter2.
2. Open the converted project data using the screen design software for GT Designer3 (GOT2000) Version 1.100E or later.
◆ GT Converter2 Version 3.14Q or later
It supports the GOT2000 series.
1. Convert the project data into GOT2000 series project data using GT Converter2.
2. Open the converted project data using the screen design software for GT Designer3 (GOT2000) Version 1.108N or later.
The GOT type of the project data is converted into GT27.
To use the project data with other models, convert the GOT type using the screen design software.
It does not support the GOT2000 series. To use the project data for GOT800 or other series with the GOT2000 series, perform the following operations.
1. Convert the project data into GOT1000 series project data using GT Converter2.
2. Open the converted project data using the screen design software for GT Designer3 (GOT2000) Version 1.100E or later.
◆ GT Converter2 Version 3.14Q or later
It supports the GOT2000 series.
1. Convert the project data into GOT2000 series project data using GT Converter2.
2. Open the converted project data using the screen design software for GT Designer3 (GOT2000) Version 1.108N or later.
The GOT type of the project data is converted into GT27.
To use the project data with other models, convert the GOT type using the screen design software.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GT Converter2
- Series
- GOT2000 Series, Engineering Software