FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 Rugged > Using the rugged model under the environment of strong external lights such as the afternoon sun
FAQ
Using the rugged model under the environment of strong external lights such as the afternoon sun
Can the rugged model be used under the environment of strong external lights such as the afternoon sun?
Answer
The rugged model can be used under the environment of strong external lights such as the afternoon sun. Make sure that the operating ambient temperature does not exceed the specifications in the afternoon sun.
Since a high-intensity liquid crystal display panel is installed, the screen is displayable on the rugged model even in the bright places such as in the afternoon sun.
The brightness is adjustable in 32 levels.
Exposure to UV for a long time may turn the GOT front face in yellow.
Use the UV protective sheet (option) if the rugged model may be exposed to UV for a long period.
Since a high-intensity liquid crystal display panel is installed, the screen is displayable on the rugged model even in the bright places such as in the afternoon sun.
The brightness is adjustable in 32 levels.
Exposure to UV for a long time may turn the GOT front face in yellow.
Use the UV protective sheet (option) if the rugged model may be exposed to UV for a long period.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series