FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 Rugged > Cleaning the rugged model with its power on
FAQ
Cleaning the rugged model with its power on
Can the rugged model be cleaned with its power on?
Answer
The GOT cannot be cleaned with its power on.
Turn off the power before cleaning the GOT. Check the following before cleaning.
・ The GOT is mounted to the control panel correctly.
・ The environmental protection sheet (not replaceable) is in the normal condition.
If the environmental protection sheet peels or the cleaning solution enters between the environmental protection sheet and the display section during cleaning, stop the cleaning immediately. Do not use the GOT in this condition.
This applies to the rugged model as well.
Turn off the power before cleaning the GOT. Check the following before cleaning.
・ The GOT is mounted to the control panel correctly.
・ The environmental protection sheet (not replaceable) is in the normal condition.
If the environmental protection sheet peels or the cleaning solution enters between the environmental protection sheet and the display section during cleaning, stop the cleaning immediately. Do not use the GOT in this condition.
This applies to the rugged model as well.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series