FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 Rugged > Using a USB interface on the control panel side of the rugged model
FAQ
Using a USB interface on the control panel side of the rugged model
Can I use a USB interface on the control panel side of the rugged model?
Answer
You can use a USB interface on the control panel of the rugged model by using the panel-mounted USB port extension.
・ GT14-C10EXUSB-4S: Cable for routing the USB interface (host) on the GOT rear face to the control panel side (front side)
・ GT10-C10EXUSB-5S: Cable for routing the USB interface (device) on the GOT rear face to the control panel side (front side)
* The panel-mounted USB port extension does not conform to IP66F.
・ GT14-C10EXUSB-4S: Cable for routing the USB interface (host) on the GOT rear face to the control panel side (front side)
・ GT10-C10EXUSB-5S: Cable for routing the USB interface (device) on the GOT rear face to the control panel side (front side)
* The panel-mounted USB port extension does not conform to IP66F.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model, cable
- Series
- GOT2000 Series