FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Using the rugged model in rain
FAQ
Using the rugged model in rain
Can the rugged model be used in rain?
Answer
The front face of the rugged model conforms to IP66F and IP67F.
Therefore, the rugged model can be used in rain when the following conditions are satisfied.
・ perating ambient temperature -20°C to 65°C
・ Operating ambient humidity 10% RH to 90% RH, non-condensing
When raindrops hit the control panel hard, the touch switch may malfunction. Do not expose the operation panel to raindrops.
Avoid using the GOT in the environment of high humidity all the time.
Therefore, the rugged model can be used in rain when the following conditions are satisfied.
・ perating ambient temperature -20°C to 65°C
・ Operating ambient humidity 10% RH to 90% RH, non-condensing
When raindrops hit the control panel hard, the touch switch may malfunction. Do not expose the operation panel to raindrops.
Avoid using the GOT in the environment of high humidity all the time.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series
May I have your opinion?
Related FAQ
- Improved UV resistance of the rugged model
- Checking the simultaneous 2-point press switches placed on the screen design software
- Compatibility of communication units for the GOT1000 series
- Location of the terminating resistor setting switch for the RS-422/485 communication port
- Operating the screen with the gesture function while using the SoftGOT-GOT link function