FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Surface treatment of the front face of the rugged model
FAQ
Surface treatment of the front face of the rugged model
What is the surface treatment of the front face of the rugged model?
Answer
The surface treatment of the front face of the rugged model is the AG (antiglare) treatment for both the environmental protection sheet and optional UV protective sheet.
The environmental protection sheet and optional UV protective sheet are made from UV cutoff materials. (95% UV cutoff with a sheet of 370nm)
The environmental protection sheet and optional UV protective sheet are made from UV cutoff materials. (95% UV cutoff with a sheet of 370nm)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model, GOT function (UV protective sheet)
- Series
- GOT2000 Series