FAQ


FAQAbout Products
- FAQ > Medium-voltage Power Distribution Products > Protection Relays > Protection Relays - MELPRO-A Series > The viewpoint of the definite time factor characteristic graph
FAQ
The viewpoint of the definite time factor characteristic graph
What do the figures on the horizontal axis of the definite time factor characteristic graph mean?
Answer
It means multiples of the settling value. For example, when a definite time factor operation settling value of a relay is 3 A, 1x is read as 3 A and 5x is read as 15 A.
- Product Name
- Protection Relay
- Series
- MELPRO-A Series