FAQ


FAQAbout Products
- FAQ > Medium-voltage Power Distribution Products > Protection Relays > Protection Relays - MELPRO-A Series > The operating time of the instantaneous factor operating characteristics
FAQ
The operating time of the instantaneous factor operating characteristics
Does the operating time of the instantaneous factor become 50 ms or shorter in both cases for 200% and 400% of the settling value?
Answer
That is right. Standard JIS C 4602 defines it shall be 50ms or shorter when 200% of the settling value is input.
- Product Name
- Protection Relay
- Series
- MELPRO-A Series