FAQ


FAQAbout Products

- FAQ > Medium-voltage Power Distribution Products > Protection Relays > Protection Relays - MELPRO-A Series > The application of the overcurrent relay
FAQ
The application of the overcurrent relay
Is that operable if one unit is connected to R-phase and another unit is connected to T-phase?
Answer
It is possible. Connect R-phase to the terminal for R-phase of the relay, and T-phase to the terminal for T-phase of the relay. And the direction of a current from the CT must be aligned for R-phase and T-phase respectively.
- Product Name
- Protection Relay
- Series
- MELPRO-A Series