FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Comparison result of the CMP instruction
FAQ
Comparison result of the CMP instruction
When the CMP instruction is executed, the comparison result is not cleared even after the command input turns off.
- Category :
Answer
A comparison result is held even after the command input turns off. The remaining comparison result can be cleared by using the RST or ZRST instruction.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series