FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Earth Leakage Circuit Breakers > 4-pole type in 100VAC or 110VAC
FAQ
4-pole type in 100VAC or 110VAC
Is it possible to use 4-pole type NV125-SV, NV125-HV, NV250-SV and NV250-HV in 100VAC or 110VAC circuit?
Answer
The rated operational voltages for them are 200 to 440VAC. If using them in 100VAC or 110VAC circuit, earth-leakage protection does not operate.
- Product Name
- Earth Leakage Circuit Breakers
- Series
- WS-V