FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Support of the DHCP (Dynamic Host Configuration Protocol) function by the FX3U-ENET-L (for Ethernet communications)
FAQ
Support of the DHCP (Dynamic Host Configuration Protocol) function by the FX3U-ENET-L (for Ethernet communications)
Does the FX3U-ENET-L support the DHCP function?
- Category :
Answer
The FX3U-ENET-L does not support the DHCP function. Set the fixed IP address using FX Configurator-EN-L. (FX Configurator-EN-L can be downloaded from Mitsubishi Electric Factory Automation website.)
On FX Configurator-EN-L, select "Ethernet settings" and "Operational settings", and set the fixed IP address.
On FX Configurator-EN-L, select "Ethernet settings" and "Operational settings", and set the fixed IP address.
- Product Name
- FX3U-ENET-L
- Product Category
- Network/Communication
- Series
- FX3U, FX3UC