FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Positioning blocks/module that can be connected with a manual pulse generator
FAQ
Positioning blocks/module that can be connected with a manual pulse generator
Are there any positioning blocks/modules which can be connected with a manual pulse generator in the FX programmable controllers? What are their input types?
Answer
The FX3U-20SSC-H (differential line driver), FX2N-10PG (differential line driver or open collector: only 5 V type), and FX2N-10GM/FX2N-20GM (open collector) are available.
- Product Name
- MELSEC-F Series
- Product Category
- FX2N, FX2NC, FX3U, FX3UC
- Series
- Positioning Control