FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Selection of analog inputs
FAQ
Selection of analog inputs
Is it possible to connect different types of analog inputs to individual channels at the same time? For example, 7 channels are used for thermocouple K type and 1 channel is used for 0-10 V DC.
Answer
The analog input type (temperature/voltage/current) and offset/gain can be set for each channel.
- Product Name
- MELSEC-F Series
- Product Category
- FX2N, FX2NC, FX3U, FX3UC
- Series
- Analog Control