FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Pulse output type of the FX3U-1PG pulse output block
FAQ
Pulse output type of the FX3U-1PG pulse output block
What is the pulse output type of the FX3U-1PG?
Answer
It is transistor output.
Transistor output specifications are as follows.
・ Rated load voltage 5 to 24 V DC
・ Maximum load current 20 mA or lower
Transistor output specifications are as follows.
・ Rated load voltage 5 to 24 V DC
・ Maximum load current 20 mA or lower
- Product Name
- MELSEC-F Series
- Product Category
- FX3U,FX3UC
- Series
- Positioning Control