Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 25222
  • Release Date : 2019/09/02 16:01
  • Print

Regarding failure of communication with MI5122-VW via Ethernet

Communication failed with MI5122-VW via Ethernet, what shall I check?
Category : 

Answer

Check the IP address of the connected device for a duplicate IP address.
If your computer has multiple network connections, check that there are no devices with the same IP address
for network connections other than those to which the MI5122-VW is connected.
Product Name
MELIPC
Series
MI5000

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries