Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 45230
  • Release Date : 2025/10/22 16:50
  • Print

Simulation function of GT Works3

Answer

GT Works3 has a simulation function. 
When GT Designer3, included with GT Works3, is installed, the simulation function (GT Simulator3) is installed simultaneously. 
You can launch the function from GT Designer3 or independently from GT Simulator3. 
* To use GT Simulator3, a PLC CPU or controller simulator is required. 
* When using a controller simulator, prepare GX Works3, GX Works2, GX Simulator, or MT Developer2. (The required software depends on the PLC CPU to be simulated.)

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GT Works3, GT Simulator3
Series
GOT Screen Design Software, Simulation Software

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries