• No : 20770
  • Release Date : 2018/08/21 16:10
  • Update : 2018/09/03 17:15
  • Print

About China CCC certification

Has the GM-J2 series received CCC certification?
Category : 

Answer

We have not acquired China's CCC certification for the GM-J2 series.
"Small-power motors" are among the products covered by China's CCC certifications (GB12350-2009), these are motors of 1.1kW or lower. The GM-S, D, SHY, and SSY series have been certified for the 0.1 to 0.75kW range.
Product Name
Geared Motors
Series
Geared Motors Parallel shaft type, Geared Motors Right angle shaft type