- No : 20851
- Release Date : 2018/08/22 16:24
-
Print
Frequency setting by the CC-Link
When the frequency is set via the CC-Link, is the frequency setting value set with the PU (operation panel) changed?
- Category :
-
Answer
When the frequency setting value is written by the CC-Link to EEPROM, the frequency setting value set with the PU (operation panel) is changed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, FR-E700, FR-E700EX