- No : 20862
- Release Date : 2018/08/22 16:24
- 
          
              Print
          
        
 
Replacement with the FR-B, B3 (A800 specification)
    
      In the document for the replacement of the A500 base with the A800 base or the A700 base with the A800 base, it is described that some functions have restrictions. What are the restrictions? 
    
  
    - Category : 
- 
      
    
 
    Answer
  
    In the A800 base of the FR-B and FR-B3, the Easy setup wizard is not available. Thus, some functions are restricted. 
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-B/B3(A800)