- No : 20896
- Release Date : 2018/08/22 16:24
-
Print
Trace function
When the data is acquired in the record mode of the trace function, two files, ST1 and TR1, are saved. What are these files?
- Category :
-
Answer
The ST1 is a setting file and the TR1 is a waveform file.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800