• No : 20896
  • Release Date : 2018/08/22 16:24
  • Print

Trace function

When the data is acquired in the record mode of the trace function, two files, ST1 and TR1, are saved. What are these files?
Category : 

Answer

The ST1 is a setting file and the TR1 is a waveform file.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800