- No : 20907
 
      - Release Date : 2018/08/22 16:25
 
        - 
          
              Print
          
        
 
  
 
PLC function
    
      On what condition does the PLC function device: SM1217 turn ON? 
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Vector control: The SM1217 turns ON when the motor rotates even if no forward rotation command is send. Other than vector control: The SM1217 turn ON by forward rotation + RUN (output frequency). 
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-A800, FR-F800