- No : 20926
- Release Date : 2018/08/22 16:25
-
Print
FR-A800-R2R
Are there any devices other than the inverter required for the tension control dedicated to winding/unwinding?
- Category :
-
Answer
A tension sensor such as a dancer roll is required for speed control. Because an actual line speed input is required for the winding diameter calculation by the actual line speed method, devices such as a speed detection device is required.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800 Plus