• No : 20927
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800-R2R

How accurate (faulty) is the winding diameter? How faulty is it for the line speed command?
Category : 

Answer

It depends on machine specifications. It depends on the accuracy of the line speed input and parameter setting of material thickness.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800 Plus