• No : 20928
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800-R2R

Is Real sensorless vector control available?
Category : 

Answer

Yes, it is. However, it is not suitable for the low speed regenerative side. It is also recommended to use a dedicated control for winding/unwinding applications that require accuracy. (dancer feedback speed control, tension sensor feedback speed control, tension sensorless torque control, and tension sensor feedback torque control)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800 Plus