- No : 20928
- Release Date : 2018/08/22 16:25
-
Print
FR-A800-R2R
Is Real sensorless vector control available?
- Category :
-
Answer
Yes, it is. However, it is not suitable for the low speed regenerative side. It is also recommended to use a dedicated control for winding/unwinding applications that require accuracy. (dancer feedback speed control, tension sensor feedback speed control, tension sensorless torque control, and tension sensor feedback torque control)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800 Plus